Zoro Homepage
Published: 5/13/2025
- Zoro Staff
- 4 min read
How to Set Up OSHA-Compliant Jobsite Hydration Stations

Keeping crews hydrated on outdoor jobsites supports OSHA compliance and may contribute to team safety and productivity. For safety managers, contractors, and site supervisors, setting up a reliable hydration station can make a real difference when it comes to managing heat and keeping work moving. This guide breaks down how to build an OSHA-compliant hydration setup using water coolers, hydration backpacks, and portable water options.

OSHA Rules for Staying Hydrated on the Job

To help prevent heat-related illness, OSHA requires employers to provide easy access to clean drinking water, rest breaks, and shade. According to standard 29 CFR 1926.51, each worker should have access to about one quart (0.95 liters) of water every hour when working in hot conditions. 

You may also want to consider providing electrolyte replenishments to your workers. When it’s hot out, water alone might not be enough. Adding electrolyte options to a hydration setup—such as tablets or powdered mixes—may assist with mineral replenishment during extended periods of exertion in the heat.

Quick Tip: Use clearly labeled hydration station signs to make water sources easy to find and encourage frequent use.

Picking a Hydration Station That Works for Your Crew

Whether you're using insulated coolers, portable dispensers, or hydration packs, the key is choosing gear that fits your team’s needs and the demands of the jobsite.

Water Coolers

Insulated water coolers help keep drinking water cold for hours, even in direct sun, and many come with spigots for quick, sanitary refills. These products are designed for durability and portability in jobsite conditions, offering crews access to clean water as needed.

Portable Hydration & Cooling Options

Need something light for a short task? A compact hydration pack can do the trick. Working long hours in the heat? Go with a larger pack that holds more water and stays comfortable throughout the day.

Hydration PacksLunchbox CoolersReusable Water BottlesCooling VestsCooling Neck Wraps

What to Look for in Hydration Station Gear

Whether it’s a water cooler, hydration pack, or portable dispenser, here are some jobsite-ready features to keep in mind.

  • Easy-dispense spigots for quick, no-fuss water access
  • Insulated containers with ice packs to keep water cool all shift long
  • Refill indicators or gauges so it’s easy to keep track of water levels
  • Reinforced water bladders for hydration packs that can handle tough conditions
  • Gear compatibility with harnesses, belts, or PPE for all-day wear without the hassle

How to Plan for Crew Water Needs

When the heat’s on, hydration needs go up. OSHA recommends each worker drink 24–32 ounces of water per hour in high temps—that’s about 2 to 3 liters during a full shift. To keep up, your hydration station setup should match your crew size, workload, and the weather.

  • Size it right: Use refillable coolers or dispensers in busy areas to keep water accessible for the whole crew.
  • Stay stocked: Assign someone to keep an eye on water levels and handle refills before supplies run low.
  • Stay mobile: Move portable hydration stations as needed so they’re always close to the action.

Hydration Station Upkeep: Cleaning and Safety Basics

Clean, safe drinking water isn’t just good practice—it’s an OSHA requirement. Under standard 1910.141, all jobsite drinking water must be stored in sanitary, clearly labeled containers to help prevent contamination.

Keeping hydration stations in good shape doesn’t have to be complicated. Here are a few simple ways to stay on top of maintenance.

  • Clean coolers and dispensers daily with food-safe disinfectants to help prevent bacteria buildup.
  • Empty and rinse the water bladder after every use. Use mild soap or dedicated cleaning tablets, then let it air-dry fully before storing.
  • Set up a maintenance checklist to track cleanings and refills—and assign a team lead to keep things running smoothly.

Getting Your Crew Hydration-Ready

A well-stocked hydration station may support OSHA compliance and contribute to crew comfort and productivity. Ready to set one up? Explore hydration gear at Zoro.com and find the supplies that work as hard as your crew does.

Product Compliance and Suitability

The statements contained in this guide are intended for general informational purposes only. Such statements do not constitute a product recommendation or representation as to the appropriateness, accuracy, completeness, correctness, or currentness of the information provided. Information provided in this guide does not replace the use by you of any manufacturer instructions, technical product manual, or other professional resource or adviser available to you. Always read, understand, and follow all manufacturer instructions. Portions of this article were generated in part by ChatGPT, and edited by a member of the Zoro team.

Related Articles