Zoro Homepage
Published: 4/4/2025
- Zoro Staff
- 4 min read
Band Saw Blade TPI Chart and Selection Guide for Wood and Metal Cutting

Selecting an appropriate band saw blade can support effective cutting performance, whether you're working in a small workshop or managing large-scale operations in manufacturing or construction. One of the most important factors to consider is TPI, or Teeth Per Inch, which directly impacts cut quality, speed, and efficiency.

In this guide, we’ll break down everything you need to know about sizes and how to use a TPI chart to select the ideal blades for your material, whether it’s wood, metal, or plastic.

What Is TPI and Why Does It Matter for Band Saw Blades?

TPI measures the number of teeth on a blade per inch of length. It’s one of the most important variables in selecting a blade suited to your application. TPI determines:

  • How smooth your cut will be
  • How fast you can cut
  • The types of materials you can efficiently cut

For example:

  • Higher TPI blades (14-24 TPI) produce smoother, slower cuts, ideal for thin materials or when a clean finish is critical.
  • Lower TPI blades (3-6 TPI) cut faster but leave a rougher edge, which is best for thicker, softer materials like hardwoods.

When selecting a band saw blade, matching the TPI to the material type and thickness is key to preventing blade damage and ensuring precision.

Band Saw Blade TPI Chart: Quick Selection Guide

The following chart offers a quick reference for choosing the correct TPI for wood, metal, and other materials. It's based on material type and thickness to help you make an informed decision.

MaterialMaterial ThicknessRecommended TPI
Wood (Hardwood/Softwood)Under 1/2" (12 mm)
1/2" to 3" (12 mm - 75 mm)
Over 3" (75 mm)
10 - 14 TPI
6 - 10 TPI
3 - 6 TPI
AluminumUnder 1/4" (6 mm)
Over 1/4" (6 mm)
14 - 24 TPI
6 - 10 TPI
Mild SteelThin-walled tubing
Solid bar stock
14 - 18 TPI
6 - 10 TPI
Stainless SteelSheet metal
Solid material
18 - 24 TPI
8 - 12 TPI
Plastics/AcrylicThin sheets
Thick blocks
10 - 14 TPI
6 - 10 TPI

How Many Teeth Should Be in the Cut?

One fundamental rule when selecting blades is ensuring you always have at least 3 teeth in contact with the workpiece during cutting. Too few teeth can cause:

  • Tooth straddling
  • Snagging
  • Tooth breakage

Too many teeth engaged can result in:

  • Overloaded gullets
  • Heat buildup
  • Slower cutting speeds

To support effective cutting, it is generally recommended to follow the 3-tooth minimum rule and consult a band saw blade TPI chart to confirm the correct TPI for your material’s thickness.

Common TPI Selection Challenges

  • Challenge #1: Selecting a coarse TPI for thin materials. This may contribute to snagging, rough edges, or premature tooth wear.
  • Challenge #2: Choosing a fine TPI for thick stock. In some cases, this can slow cutting performance, reduce gullet efficiency, or generate excess heat.
  • Challenge #3: Not accounting for the "3-teeth-in-the-cut" guideline. This may affect cutting efficiency and blade longevity.

Understanding Band Saw Blade Sizes

It’s important to understand band saw blade sizes and how they impact your cut. Band saw blade size includes three dimensions:

  1. Blade Length – This must match your machine’s specifications.
  2. Blade Width – Affects your ability to make straight or curved cuts.
  3. Blade Thickness – Impacts durability and resistance to bending or breaking.

Once you have the right band saw blade size, choosing the correct TPI count supports reliable cutting. 

How to Measure a Band Saw Blade

If you're unsure about your blade’s specs, here's how to measure a band saw blade properly.

  1. Length: Use a flexible tape measure around the blade's circumference or consult your machine's manual.
  2. Width: Measure from the back of the blade to the tip of the teeth.
  3. Thickness: Use a caliper for an accurate measurement.
  4. TPI (Teeth Per Inch): Count the number of teeth over a 1" span on the blade.

Knowing how to measure a band saw blade ensures you always order the correct size for your saw.

Selecting the right band saw blade TPI is an important step in achieving consistent, accurate cuts across different materials. By understanding how blade size, TPI, and material thickness interact, professionals can make informed choices that support cutting efficiency and tool longevity. Explore our full selection of band saw blades to find options aligned with your cutting needs.

Product Compliance and Suitability

The statements contained in this guide are intended for general informational purposes only. Such statements do not constitute a product recommendation or representation as to the appropriateness, accuracy, completeness, correctness, or currentness of the information provided. Information provided in this guide does not replace the use by you of any manufacturer instructions, technical product manual, or other professional resource or adviser available to you. Always read, understand, and follow all manufacturer instructions. Portions of this article were generated in part by ChatGPT, and edited by a member of the Zoro team.

Related Articles