Zoro Homepage
Clipboard Icon Quick Order Cart Icon 0 Cart
Updated: 3/20/2026
- Zoro Staff
- 3 min read
Building Construction Types Explained: Fire-Resistance Ratings and Safety Standards

If you’re a contractor or business owner in construction, you know that choosing the right materials impacts safety, compliance, and performance. Building construction types—and their fire-resistance ratings—play a key role in meeting various codes and protecting your property. This guide explains the five IBC (International Building Code) and NFPA construction types, how fire ratings are determined, and what those classifications mean for your jobsite.

What Are Fire-Resistance Ratings?

Fire-resistance ratings, also called fire ratings, measure how long a building material or assembly can withstand exposure to fire before losing its structural integrity. Common materials like concrete, gypsum, and steel are tested under controlled conditions by organizations such as Underwriters Laboratories (UL) and the National Fire Protection Association (NFPA).

These ratings help ensure that:

  • Buildings contain a fire long enough for occupants to evacuate safely
  • Flames don’t spread to nearby structures
  • Property damage is minimized

Fire ratings are typically expressed in one-hour, two-hour, or three-hour increments, based on performance in standardized testing.

How Are Fire Ratings Determined?

During laboratory testing, materials are exposed to intense heat to evaluate:

  • Structural integrity—ability to bear loads under fire conditions
  • Fire containment—ability to block heat and smoke spread
  • Temperature transmission—how much heat transfers to adjacent areas

Results guide manufacturers and contractors in selecting materials that meet fire safety codes and insurance requirements.

Building Construction Types (NFPA & IBC Types I–V Explained)

Construction TypeDescriptionTypical UseFire Resistance
Type I – Fire-ResistiveMade from concrete and protected steelHigh-rise or commercial buildings3–4 hours
Type II – Non-CombustibleReinforced masonry or metal framingLarge retail or warehouse facilities1–2 hours
Type III – OrdinaryNon-combustible walls with wood roofsSchools, mixed-use structures1 hour
Type IV – Heavy TimberLarge wood beams with slow burn rateHistoric mills, barns, churches1 hour
Type V – Wood-FramedLight wood framing, most cost-effectiveResidential or small commercial<1 hour

Each classification includes subtypes (IA/IB, IIA/IIB, etc.) defining minimum fire-resistance ratings for walls, floors, and framing systems.

Fire Rating Classes for Materials

Materials are further grouped by flame spread and smoke development indexes.

  • Class A (highest resistance): Flame spread ≤25, smoke ≤450
  • Class B (moderate resistance): Flame spread 26–75, smoke ≤450
  • Class C (suitable for low-risk areas): Flame spread 76–200, smoke ≤450

These classifications help identify which materials meet fire-safety needs for your application.

How to Find Fire Ratings for Building Materials

  1. Check manufacturer specifications. Fire ratings are published for most materials, including drywall, steel, and insulation.
  2. Use UL and NFPA tables. Both organizations publish detailed fire-resistance charts.
  3. Review tested assemblies. Walls and ceilings are often rated as full systems rather than individual materials.

Designing for Fire Safety

Your construction type determines baseline fire-resistance requirements. For example:

  • Type IA office towers may require 3-hour structural frames.
  • Type IIB warehouses may use 1-hour-rated steel systems.
  • Type VB homes depend on drywall or coatings to add protection.

Installation is equally important. Gaps or improper seals can reduce a wall’s fire rating. Always ensure rated doors, windows, and penetrations match the assembly’s certification.

Wrapping It Up

Understanding construction types and fire ratings helps ensure safety, compliance, and efficiency on every jobsite. Whether you’re managing new builds or renovations, selecting fire-rated materials that align with your project’s classification supports both protection and peace of mind. At Zoro, we make it easier to find the materials and tools you need to stay compliant and keep your crew safe so you can focus on getting the job done.

Product Compliance and Suitability
The statements contained in this guide are intended for general informational purposes only. Such statements do not constitute a product recommendation or representation as to the appropriateness, accuracy, completeness, correctness, or currentness of the information provided. Information provided in this guide does not replace the use by you of any manufacturer instructions, technical product manual, or other professional resource or adviser available to you. Always read, understand, and follow all manufacturer instructions. Portions of this article were generated in part by ChatGPT, and edited by a member of the Zoro team.

Related Articles