Zoro Homepage
Clipboard Icon Quick Order Cart Icon 0 Cart
Updated: 1/28/2026
- Zoro Staff
- 4 min read
Choosing the Right Tankless Water Heater for Your Small Business

What Is a Tankless Water Heater?

As a business owner, hot water can be an indispensable part of your work, from washing dishes in a hospitality setting to ensuring you have the water supply needed for hygienic bathrooms and sanitizing equipment. From restaurants and commercial kitchens to hospitals, clinics, and universities, many spaces are unable to function without hot water. But what if your business could ensure a steady supply of hot water without the downsides of a typical water heater? 

Enter tankless water heaters, also known as on-demand water heaters. These innovative hot water heaters provide hot water on demand without the need for a storage tank—with benefits for your business that include greater efficiency, less space taken up by the equipment, and tech advancements that make it easier to remotely monitor your water use. Here, we'll take a closer look at commercial tankless water heaters so you can decide for yourself whether they're the right choice for your small business.

Types of Tankless Water Heaters

When shopping for a tankless water heater, you'll need to decide whether you want to implement a gas or electric water heater. As with other appliances, the choice will depend on your needs and the existing utility supplies in your space, among other considerations.

Gas Tankless Water Heaters Electric Tankless Water Heaters
Gas Tankless Water Heater Electric Tankless Water Heater

 

Benefits of Using a Tankless Water Heater for Your Business

Energy Efficiency

Illustration of a dial with a lightning bolt on it. Two arrows circle around the dial in a counterclockwise direction.

The most significant benefit of using a tankless water heater is the reduction in energy costs due to greater efficiency, which is especially important for business owners who must always manage the bottom line. Traditional water heaters store hot water in a tank and require continuous heating. A tankless water heater, on the other hand, only heats water as needed, resulting in a significant energy savings for your business. According to Engineered Systems Magazine, tankless propane water heaters have the potential to use 25% less energy than conventional heaters and can save your business a significant amount of money on electric bills each year.

Space Saving

Illustration of an unrolled floor plan document

While traditional water heaters may take up a significant amount of space in your business, tankless water heaters are compact and can be mounted on the wall. Of course, this will help free up valuable floor space in your business, which is especially important in compact spaces where every square foot counts.

On-Demand Hot Water

Illustration of a water tap with a drop coming out

When it comes to tankless water heaters, the benefits aren't limited to just energy and space savings. With traditional water heaters, there is always a limit to the supply of hot water available, as the tank can only hold a certain amount of water. This can be a problem for businesses with high hot water demands. Tankless water heaters provide an endless supply of hot water, ensuring that your business can meet high hot water demands on busy days.

Technological Advancements

Image of a cell phone displaying a drop of water on the screen. Curved lines around the phone indicate a wireless signal.

Commercial tankless water heaters are often equipped with new technologies such as cellular and Wi-Fi connectivity, allowing you to remotely monitor factors such as water flow and water temperature. For business owners on the go, these features can make it easier to check in on your business and keep everything running smoothly when you're away from the space.

Hot water is essential for a wide variety of businesses—and if you're investing in a new water heater, it's worth considering whether tankless options are right for you. Commercial tankless water heaters can not only save you money, energy, and space, but they also come with advanced technologies that make it easier to keep an eye on your hot water usage. In addition, the on-demand hot water from a tankless heater may make it easier to keep up with demand without worrying that you'll exhaust your supply of hot water. 

Looking to upgrade your business with a new tankless water heater? Explore your options and find the right product for your needs at Zoro.com.

Product Compliance and Suitability

The product statements contained in this guide are intended for general informational purposes only. Such product statements do not constitute a product recommendation or representation as to the appropriateness, accuracy, completeness, correctness, or currentness of the information provided. Information provided in this guide does not replace the use by you of any manufacturer instructions, technical product manual, or other professional resource or adviser available to you. Always read, understand, and follow all manufacturer instructions.

Related Articles