Flap Disc Grit Chart
Choose the Right Grit for Metal
The Ultimate Flap Disc Grit Chart: Matching Grit to Your Metalworking Job
Using an angle grinder without understanding abrasive grit is a lot like using a chainsaw for a manicure—you might get the job done, but it’s going to be incredibly messy, and you’ll probably ruin the workpiece.
In metal fabrication, your choice of flap disc grit dictates everything. Choose a grit that is too coarse, and you will gouge deep, irreversible scars into an expensive sheet of stainless steel. Choose a grit that is too fine, and you will spend three hours trying to grind down a single weld bead, generating excess heat that warps your metal.
To get the perfect finish in the shortest amount of time, you need to understand the flap disc grit spectrum. Here is your definitive guide and reference chart to matching the right grit to your metalworking project.
The Flap Disc Grit Chart
Before we dive into the details of each grit level, here is a quick-reference guide to help you select the right abrasive size for your application.
| Grit Range | Classification | Primary Applications | Best For | Finish Quality |
|---|---|---|---|---|
| 36 – 40 | Extra Coarse | Heavy weld removal, beveling, stripping thick rust/paint | Structural steel, heavy plates | Rough, deep scratch pattern |
| 60 | Coarse/Medium | General weld blending, edge deburring, shaping | Mild steel, carbon steel | Moderate, easy to blend |
| 80 | Medium/Fine | Light blending, surface prep, scratch removal | Stainless steel, aluminum | Smooth, satin finish |
| 120+ | Ultra-Fine | Final finishing, polishing, pre-paint prep | All metals (final passes) | Highly polished, paint-ready |
Breaking Down the Grit Categories
Abrasive grit numbers refer to the size of the abrasive particles on the disc. The lower the number, the larger and more aggressive the particles. The higher the number, the smaller and finer the particles.
1. Extra Coarse: 36 to 40 Grit (The Heavy Hitters)
When you have a massive bead of structural weld to level or a thick piece of scale-covered plate steel to prep, reach for a 36 or 40-grit flap disc.
- What it does: These discs act like miniature plows. They dig deep into metal to pull away massive amounts of material in a single pass.
- Best used for: Heavy stock removal, weld leveling, beveling thick pipe or plate before welding, and ripping off thick layers of rust, scale, or old paint.
- The Catch: They leave highly visible, deep scratch patterns. You should never use a 40-grit disc on thin sheet metal or any workpiece where cosmetics matter, as you will easily gouge the material.
2. The Sweet Spot: 60 Grit (The Jack-of-All-Trades)
Ask any professional fabricator which single flap disc they would take to a desert island, and nine out of ten will say a 60-grit zirconia or ceramic disc.
- What it does: 60-grit strikes the perfect, elusive balance between rapid material removal and a manageable surface finish. It is aggressive enough to grind down standard weld beads but refined enough that you won't accidentally ruin your workpiece with a slight slip of the hand.
- Best used for: General weld cleanup, deburring sharp cut edges, removing fabrication burrs, and general-purpose shaping.
- The Catch: While it is highly versatile, you will still need to step up to a finer grit if your metal is slated for high-end paint, powder coating, or mirroring.
3. Medium to Fine: 80 Grit (The Blender)
Once your heavy grinding is finished, 80-grit is your go-to for making those transitions look seamless.
- What it does: An 80-grit disc removes very little structural metal. Instead, it focuses on shaving down the scratch marks left behind by 36 or 60-grit discs, blending the ground area flush with the surrounding metal.
- Best used for: Surface preparation before priming, blending welds on stainless steel (where appearance is critical), cleaning up light surface rust, and working on softer metals like aluminum that clog coarser discs.
- The Catch: If you try to grind down a massive, proud weld bead with an 80-grit disc, you will quickly glaze the disc over, generate massive amounts of heat, and get nowhere fast.
4. Ultra-Fine: 120 Grit and Beyond (The Finisher)
If your metal needs to look like a mirror, or if you are preparing a surface for a flawless, high-gloss paint job, 120-grit is where your process ends.
- What it does: This grit acts more like a heavy-duty polishing pad than a grinding disc. It gently buffs the metal, removing microscopic scratches and leaving behind a highly uniform, satin or semi-reflective finish.
- Best used for: Final surface finishing, removing tiny scratches, polishing stainless steel in architectural or food-grade applications, and pre-paint preparation.
- The Catch: Absolutely zero material removal capability. Use this only on surfaces that are already flat and structurally sound.
Pro-Tips for Maximizing Your Flap Discs
- The Two-Step Rule: Don't try to go straight from a 36-grit grind to a 120-grit finish. You will waste time and ruin discs. Always step down progressively (e.g., grind with 40, blend with 80, finish with 120).
- Match Your Material: Ensure you pair your grit with the right grain. Use Ceramic or Zirconia grains for hard metals like stainless steel, and Aluminum Oxide for softer steels or single-use DIY projects.
- Let the Tool Do the Work: Pushing too hard on a fine-grit disc won't make it grind faster—it will only overheat the metal, causing discoloration (bluing) on stainless steel and melting the abrasive backing.
Product Compliance and Suitability
The statements contained in this guide are intended for general informational purposes only. Such statements do not constitute a product recommendation or representation as to the appropriateness, accuracy, completeness, correctness, or currentness of the information provided. Information provided in this guide does not replace the use by you of any manufacturer instructions, technical product manual, or other professional resource or adviser available to you. Always read, understand, and follow all manufacturer instructions. Portions of this article were generated in part by ChatGPT.