Everything You Need to Know About Auto-Darkening Welding Helmets
Choosing the right type of welding helmets for your business is essential to the safety of your crew. In general, welding helmets come in two types: passive or regular-lens helmets and auto-darkening helmets. A passive helmet features a lens of standard glass coated with infrared and ultraviolet protection and serves as a one-size-fits-all option. In contrast, an auto-darkening helmet adjusts instantly when it senses an arc of welding light. Read on to learn more about auto-darkening welding helmets and why they’re the preferred choice of many expert welders.
What Are Auto-Darkening Welding Helmets?
As discussed above, auto-darkening welding helmets instantly adjust to a darker lens shade when they sense an arc of welding light. However, there’s much more to know about this high-tech personal protective equipment. Here are some highlights.
- Auto-darkening sensors provide exceptional protection across a wide variety of welding projects.
- The lens automatically adjusts back to natural light, allowing the wearer to inspect jobs without having to pull the helmet on and off.
- The helmets also provide excellent protection to the wearer’s head, face, neck, and ears.
- Auto-darkening helmets do not need to be snapped in place (a great benefit to beginner welders).
- Wearers of auto-darkening helmets only need one helmet for their welding processes.
How Does Auto-Darkening Technology Work?
Modern auto-darkening welding helmets feature the same infrared and ultraviolet protection found in passive helmets, along with filter lenses that are similar to the LCD, or liquid crystal display, found on many TVs and other appliances. In addition, each layer of protection features a polarization filter to help reduce glare. Let’s look at some additional features.
- Auto-darkening filter lenses are powered by either batteries or a combination of battery and solar power. Tiny light sensors are found near the lenses. Top-of-the-line auto-darkening helmets feature four sensors, providing maximum protection across the entire face of the shield.
- When the sensors are not activated, the lens features a level 3 or 4 shade, which is comparable to the protection provided by a high-quality pair of sunglasses in very bright sunlight.
- When the arc of light from a welding device triggers the auto-darkening technology to kick in, the lens darkens the shade to a level 10 or as high as 13, which effectively protects the eyes from almost any type of harmful ray.
- Wearing an auto-darkening helmet also brings added safety when working in dark conditions. Thanks to the technology built into its sensors, it will adjust automatically in situations where the human eye might not react to the change in brightness quickly enough to avoid eye damage.
More Factors to Consider
View and Protection
If you want to have a complete view of the work in front of you, choose a helmet with a full-coverage shell, which means it provides a clean line of sight and also covers your entire head, including the neck, scalp, ears, and face.
Control
Functionality controls can be found on either the inside or outside of the helmet, and allow the wearer to make adjustments to the shade levels as needed. External controls allow for easy shade tweaks while the helmet is on, saving time and therefore allowing for even more efficiency on the job. On the other hand, internal controls are not exposed to sparks or rough handling that can cause damage or operational failure.
Settings
Light and sensitivity controls are available in many models of auto-darkening helmets, which give welders more control over how and when the shades change, based on the details of the job or other factors. For example, if multiple welders are working at once in the same area, the shades can be set to not activate when the torches of nearby welders are lit. Some helmets also include delay controls, which can be set to delay the time it takes for the higher-level, darker shades to transition back to lower-level, lighter shades.
Power
As discussed above, some auto-darkening welding helmets are powered by standard, rechargeable, or lithium batteries only, while others feature a mix of battery and solar power. In general, helmets with replaceable batteries last longer. Non-replaceable batteries typically last between 5 and 8 years.
Comfort
A proper-fitting welding helmet should tighten easily and fit snugly around your head to ensure it stays safely in place throughout your work day. Some versions are lighter than others, which many professionals prefer over heavier models that can start to feel uncomfortable after several hours. The helmet should be balanced and secure and never wobbly while in use.
* * *
Whether you’re ready to invest in auto-darkening welding helmets today or you’re still gathering information, keep in mind that Zoro has all the welding supplies your business needs when you’re ready. Plus, find everything else your business needs from tools to office supplies today!
Product Compliance and Suitability
The product statements contained in this guide are intended for general informational purposes only. Such product statements do not constitute a product recommendation or representation as to the appropriateness, accuracy, completeness, correctness, or currentness of the information provided. Information provided in this guide does not replace the use by you of any manufacturer instructions, technical product manual, or other professional resource or adviser available to you. Always read, understand, and follow all manufacturer instructions.