Zoro Homepage
Published: 12/8/2025
- Zoro Staff
- 3 min read
How to Repair Stripped Threads: Step-by-Step Guide for Every Jobsite

When a bolt spins without tightening, it can bring work to a halt. Stripped threads show up on equipment, tooling, and structural components across construction and manufacturing sites, but they’re often repairable with a few dependable methods. This guide walks you through the common repair options, how to choose between them, and the steps to restore a secure, long-lasting connection.

What Causes Thread Damage?

Threads can wear down for several reasons.

  • Vibration that loosens hardware over time
  • Misalignment during assembly
  • Deformation from mismatched thread pitch or size
  • Corrosion in outdoor or high-moisture environments
  • Over-torquing fasteners in soft metals like aluminum

Choosing the Best Repair Method for the Job

Before selecting a repair approach, consider:

  • Metal type—Aluminum and zinc alloys wear faster and often need reinforced threads.
  • Load and torque—Higher loads call for more durable thread restoration.
  • Accessibility—Tight spaces may favor compact repair solutions.
  • Existing hole condition—Some holes can be restored, while others need enlargement.

Method 1: Using Threaded Inserts or Helicoils

Threaded inserts, including coil-style helicoils, are widely used in industrial repairs because they re-establish strong internal threads even in softer metals.

How to do it:

  • Clean the hole and remove loose material or corrosion.
  • Drill using the bit size specified in the repair kit.
  • Tap the new internal threads using the provided tap.
  • Thread the insert into the hole. For helicoils, break off the tang if required.
  • Install the bolt into the new threads.

This method supports repeated assembly and disassembly without significant wear.

Method 2: Drill and Tap to a Larger Size

If the original threads are beyond repair, tapping the hole to a slightly larger diameter can provide a secure hold.

How to do it:

  • Choose the appropriate tap and corresponding bolt size.
  • Secure the workpiece and apply cutting fluid.
  • Align the tap so it stays straight through the cut.
  • Tap slowly, reversing periodically to clear chips.
  • Test the bolt fit and torque according to your equipment requirements.

Method 3: Light-Duty or Temporary Repairs

Some situations don’t require a fully reinforced threaded connection. For low-load components, consider:

  • Installing a slightly larger screw or bolt
  • Filling the hole with metal epoxy, then drilling and tapping after it cures

Threaded Insert vs. Helicoil: What’s the Difference?

Both restore internal threads, but they aren’t the same thing.

  • Threaded insert: A general category that includes solid inserts, key-locking inserts, coil inserts, and other designs.
     
  • Helicoil: A specific type of coil-style threaded insert often used for metal repairs, especially aluminum.

Best Practices to Prevent Repeat Damage

A few maintenance habits help extend thread life.

  • Align bolts carefully during assembly to avoid cross-threading.
  • Use hardware with matching thread pitch and size.
  • Apply torque evenly and follow your equipment’s recommended torque values.
  • Add locking compounds for vibration-prone machinery.
  • Keep thread repair kits and tap-and-die sets onsite to reduce downtime (and avoid last-minute improvisation).

Final Thoughts

Stripped threads don’t have to slow down your schedule. By choosing the repair method that fits your equipment, material, and workload, you can restore a dependable connection and keep your operation moving. Zoro offers a range of thread repair kits, threaded inserts, tap-and-die tools, and cutting fluids to support your maintenance program and help you stay productive on every jobsite.

Product Compliance and Suitability

The statements contained in this guide are intended for general informational purposes only. Such statements do not constitute a product recommendation or representation as to the appropriateness, accuracy, completeness, correctness, or currentness of the information provided. Information provided in this guide does not replace the use by you of any manufacturer instructions, technical product manual, or other professional resource or adviser available to you. Always read, understand, and follow all manufacturer instructions. Portions of this article were generated in part by ChatGPT, and edited by a member of the Zoro team.

Related Articles