Zoro Homepage
Published: 8/6/2025
- Zoro Staff
- 4 min read
How to Stay Warm in a Cold Office: Practical Comfort Solutions for the Workday

Whether your office is inside a warehouse, behind a jobsite trailer, or tucked into a drafty corner of a commercial building, cold temperatures can be a real distraction. And if you’re a small business owner trying to keep your crew productive and comfortable, managing those conditions matters. Office temperatures are often controlled centrally, and they’re not always set with individual comfort in mind. That leaves many teams dealing with chilly conditions that impact focus, morale, and even performance, especially in fall and winter. If you’ve been wondering how to stay warm in a cold office, here’s a breakdown of why offices feel cold and what you can do about it, with practical, office-safe solutions that work without interrupting the job.

Why Are Office Buildings So Cold?

Most commercial spaces use centralized HVAC systems designed for efficiency across large square footage. These systems aim to balance the temperature for the average person in the average spot—typically around 71–74°F. However, factors like window exposure, HVAC vent placement, and personal metabolism mean that what’s “comfortable” varies widely.

When your office runs cooler than most, adding simple comfort measures can help bridge the gap without adjusting the whole system.

How to Stay Warm in a Cold Office: Simple, Effective Strategies for Staying Comfortable at Work

Here are some objective, proven ways to keep warm at your desk, with no rewiring or structural changes required.

1. Bring Layers You Can Adjust

Light jackets, thermal undershirts, and sweaters help regulate body heat without overheating. If you’re moving in and out of different temperature zones (say, between an office and the shop floor), wearing removable layers can make the transition easier.

2. Use Fingerless Gloves for Typing

If you or your admin staff spend long hours at the keyboard, fingerless gloves keep your hands warm while leaving dexterity intact. Look for styles with soft, breathable fabrics that won’t restrict movement or irritate skin.

3. Keep Warm Beverages at Your Desk

An insulated mug with a warm drink like coffee, tea, or soup can double as a hand warmer and a steady source of heat. Smart mugs with temperature controls help keep drinks warm for hours, reducing trips to the microwave or breakroom.

4. Try a Heated Blanket or Wrap

For offices with consistent chill, a low-voltage heated blanket or wrap approved for indoor use can provide warmth directly to the body. Many options are designed with automatic shut-offs for safety, making them suitable for workplace settings.

5. Use a Desk Heater or Heating Pad

Portable desk heaters and under-desk foot warmers offer focused warmth right where you need it. Choose models that meet UL safety standards and feature built-in overheat protection.

6. Keep Your Feet Warm

Cold feet make the rest of your body feel colder. Swap out dress shoes or steel toes for insulated slippers or warm socks while seated, especially if you’re at your desk for long periods.

7. Eat Warm Meals and Stay Hydrated

Warm lunches like soups or stews can help raise internal body temperature. Staying hydrated—even with warm water—also supports healthy circulation, which plays a role in regulating body heat.

8. Move Around When You Can

Short walks or light stretches during breaks can help your body generate heat naturally. Even five minutes of movement can make a noticeable difference if you're feeling stiff or cold.

You don’t need to overhaul your HVAC system to create a more comfortable work environment. With a few thoughtful additions like heated accessories, layers, and insulated drinkware, you can help your team stay focused and warm, no matter what the building temperature says.

Product Compliance and Suitability

The statements contained in this guide are intended for general informational purposes only. Such statements do not constitute a product recommendation or representation as to the appropriateness, accuracy, completeness, correctness, or currentness of the information provided. Information provided in this guide does not replace the use by you of any manufacturer instructions, technical product manual, or other professional resource or adviser available to you. Always read, understand, and follow all manufacturer instructions. Portions of this article were generated in part by ChatGPT, and edited by a member of the Zoro team.

Related Articles