Published: 10/19/2026
- Zoro Staff
- 4 min read
Types of Gantry Cranes

Types of Gantry Cranes: The Heavyweights of Overhead Lifting

While jib cranes excel at providing dedicated, localized lifting power to a single workstation, gantry cranes are built to handle the heavy lifting across expansive areas. Unlike bridge cranes that travel on overhead runways anchored to a building's structure, a gantry crane utilizes a bridge supported by legs that travel along floor-level tracks or wheels.

From bustling shipping ports to small automotive repair shops, gantry cranes come in a wide variety of sizes and configurations. Understanding the different types of gantry cranes is essential for matching the right equipment to your specific lifting capacity, environment, and mobility needs.

1. Full Gantry Cranes

The full gantry crane is the most recognizable configuration in heavy industry. It consists of two vertical A-frame legs that travel along a fixed track or rail system embedded in the floor.

  • Capacity: Extremely high, ranging from 5 tons to over several hundred tons.
  • Mobility: Fixed to a linear track system.
  • Best Used For: Shipyards, steel yards, rail terminals, and massive outdoor manufacturing spaces where heavy raw materials need to be moved across a long, dedicated path.

Because the legs travel on a track at ground level, full gantry cranes eliminate the need for expensive overhead runway structures, making them highly efficient for outdoor applications.

2. Semi-Gantry Cranes

A semi-gantry crane is a hybrid solution that blends a traditional overhead bridge crane with a gantry crane. It features one leg that runs on a floor rail, while the other side of the bridge is supported by an overhead runway beam mounted to the building's wall or structural columns.

  • Capacity: Medium to high heavy-duty lifting.
  • Space Saving: Excellent for tight spaces because it utilizes existing building structures on one side.
  • Best Used For: Facilities where you need to save floor space or want to clear a wide walkway under one side of the crane. It is often installed below a larger, building-wide overhead crane to service individual manufacturing bays.

3. Portable Gantry Cranes

Not all lifting jobs require heavy industrial infrastructure. Portable gantry cranes are smaller, lightweight systems mounted on heavy-duty casters or wheels rather than fixed rails.

  • Mobility: Highly flexible; they can be manually rolled anywhere within a shop floor, locked into place for a lift, and then stored away when not in use.
  • Capacity: Typically ranges from 0.5 to 5 tons.
  • Best Used For: Automotive repair shops, smaller fabrication facilities, and maintenance departments where loads need to be lifted and moved occasionally across different workstations.

Many portable units feature adjustable heights and spans, making them incredibly versatile for changing workplace environments.

4. Adjustable Gantry Cranes

Adjustable gantry cranes can be either portable (on wheels) or stationary. Their defining feature is the ability to adjust the height of the legs, the span of the bridge beam, or both. This adjustment is usually achieved through a series of pin connections or mechanical jacks.

  • Versatility: Can be customized on the fly to navigate through low-clearance doorways or fit into narrow aisles.
  • Best Used For: Warehouses with varying ceiling heights, facilities that regularly change their layout, or service technicians who need to transport a crane to different job sites.

5. Rubber-Tired Gantry Cranes (RTG)

When a crane needs massive industrial lifting power but cannot be restricted to a steel rail line, Rubber-Tired Gantry Cranes (RTGs) are the ultimate solution. Instead of running on tracks, these colossal structures move on massive rubber tires, often powered by diesel generators or electric grid connections.

  • Mobility: Steerable and capable of moving freely across reinforced concrete yards.
  • Capacity: Massive, frequently handling 40 to 100+ tons.
  • Best Used For: Intermodal shipping ports for stacking shipping containers, and large precast concrete yards.

Choosing the Right Gantry Crane: A Quick Comparison

Crane TypeMobilityTrack Required?Typical CapacityPrimary Environment
Full GantryFixed linear pathYesVery High (Up to 500+ tons)Outdoor yards, shipyards
Semi-GantryFixed linear pathYes (One side)High (Up to 50+ tons)Indoor manufacturing bays
Portable360° manual rollingNo (Casters)Low (0.5 to 5 tons)Machine shops, garages
AdjustableFlexible/VariableNoLow to MediumFacilities with tight clearances
Rubber-Tired (RTG)Steerable mobilityNoMassive (Container handling)Shipping ports, rail yards

Selecting the right gantry crane depends entirely on your operational footprint and the weight of your loads. For light-duty, flexible shop maintenance, a portable or adjustable gantry keeps your workflow agile. For heavy manufacturing and shipping logistics, a full, semi, or rubber-tired gantry provides the structural muscle required to move the world's heaviest cargo safely and efficiently.

Product Compliance and Suitability

The statements contained in this guide are intended for general informational purposes only. Such statements do not constitute a product recommendation or representation as to the appropriateness, accuracy, completeness, correctness, or currentness of the information provided. Information provided in this guide does not replace the use by you of any manufacturer instructions, technical product manual, or other professional resource or adviser available to you. Always read, understand, and follow all manufacturer instructions. Portions of this article were generated in part by ChatGPT.