Zoro Homepage
Published: 9/14/2023
- Zoro Staff
- 5 min read
Why Safety Nets Are Crucial in Any Industry

Safety nets come in a variety of shapes and sizes, depending on the application they are intended for. Standard safety nets include horizontally spanned safety nets, guard rail nets, vertically tensioned nets, cover nets, animal protection nets, and leaf netting. It’s important to select the right type of safety net for the application and install it correctly to ensure maximum protection against falls from heights and other potential hazards, such as falling objects or debris entering enclosed spaces below.

Benefits of Safety Netting

Safety netting is an absolute must-have in any situation with a risk of falling or other serious injuries. It's not just an optional extra - it's a crucial element that provides protection and can help prevent accidents and keep people safe. Whether you're working on a construction site or any other high-risk environment, it's imperative to ensure that proper safety netting is in place. Always remember that safety should be your top priority, and taking the necessary precautions can make all the difference in preventing accidents and saving lives.

Types of Safety Netting Uses

Industrial Safety Netting

  • Serves a variety of purposes in different industries

Debris Safety Netting

  • Used in construction sites to protect workers, equipment, and structures from falling debris

Lifting Cargo Nets

  • Used for load transportation to ensure safety and security

Machine-guarding Safety Nets

  • Protect equipment from debris and dust, ensuring longevity and efficiency

Knotless Netting

  • Used to secure items during transport, providing stability and security

Dielectric Safety Netting

  • Protects against electrical hazards in power stations, mining, and tunneling construction

Rockfall Safety Nets

  • Prevent accidents and injuries caused by falling rocks in construction sites

Ice Fall Safety Nets

  • Provide additional protection on winter worksites

Pallet racket netting

  • Used in warehouses and logistics centers to secure goods on pallets during storage or shipping.

Understanding the Uses of Safety Nets Across Different Industries

Safety nets are an essential tool for providing protection against falls from heights and other hazards in a variety of industries. From hospitals to construction sites, housing developments to recreation areas and landing docks, safety netting can be used to ensure maximum safety for workers and visitors alike.

Hospitals

In hospitals, safety netting can be used around beds and medical equipment to prevent patients from accidentally rolling off beds onto hard surfaces below them. This is an important measure for ensuring the safety of patients and avoiding potential injury or death.

Construction Sites

At construction sites, safety netting can be used around scaffolding structures as well as open pits where workers may need access but could potentially fall into if not properly protected. Guard rail nets should be installed around scaffolding structures and open pits to ensure maximum safety for workers onsite.

Housing Developments

In housing developments, safety netting can be used around balconies, roofs, and windowsills where people may need access but could fall off if not adequately protected. Installing safety nets in these areas is essential for preventing falls from heights which could result in severe injury or death.

Recreation Areas and Trampolines

Safety netting can protect visitors from potential falls or accidents in recreational areas such as playgrounds or swimming pools. Covernets should be installed over trampolines, guardrail nets should be installed around playgrounds, and leaf netting should be placed over swimming pools to ensure maximum protection against falls or accidents in these areas.

Landing Docks

At landing docks, vertically tensioned nets should be installed along walls surrounding dockside areas where people may need access but could fall into the water if not properly protected with proper safety measures. This is an essential measure for ensuring the safety of those accessing the area while avoiding potential injury or death due to falls into the water below them.

Properly Installing Safety Nets According to OSHA Regulations

When installing safety nets, it is important to follow OSHA regulations to ensure proper installation and maximum protection against falls from heights and other hazards. Make sure to select the right type of safety net for the application, determine the required height for maximum protection, and install the safety net according to OSHA standards.

Here are a couple of Osha regulations to keep in mind:

  1. Identify the area where you need to install safety nets and determine the appropriate type of netting.
  2. Ensure the netting meets OSHA requirements for strength, height, and installation methods.
  3. Install the safety netting according to OSHA regulations, which require that it be attached securely to a structure at least 6 feet above any adjacent lower level and have a minimum breaking strength of 2,500 pounds per square foot or 1,800 pounds per linear foot.
  4. Inspect the safety nets regularly to ensure they are in good condition and properly installed.
  5. Train employees on safely using and inspect safety nets before allowing them to work near them.
  6. Document all inspections and maintenance activities related to the safety nets to comply with OSHA record-keeping requirements.

Product Compliance and Suitability

The product statements contained in this guide are intended for general informational purposes only. Such product statements do not constitute a product recommendation or representation as to the appropriateness, accuracy, completeness, correctness, or currentness of the information provided. Information provided in this guide does not replace the use by you of any manufacturer instructions, technical product manual, or other professional resource or adviser available to you. Always read, understand, and follow all manufacturer instructions. Portions of this article were generated in part by ChatGPT, and edited by a member of the Zoro team.

 

Related Articles