Zoro Homepage
Published: 9/14/2023
- Zoro Staff
- 5 min read
The Types of Wire Strippers & How to Use Them

Types of Wire Strippers

The Wire Stripper and Cutter

This multipurpose tool is ideal for working with multiple wires in different sizes. It features adjustable blades and a comfortable grip for easy use.

Gauged Automatic Wire Strippers

These are designed to quickly and accurately strip the insulation off of electrical wires. They feature a gauge that allows for precise stripping of different sizes, making them great for electricians or anyone who needs to work with multiple wires in a single project.

Self-Adjusting Strippers

These are designed to adjust size to fit the wire being stripped automatically. They also feature an ergonomic design for comfortable use, making them great for quickly stripping multiple wires without having to adjust the tool each time manually.

Gauged Strippers

Similar to Gauged Automatic Wire Strippers, these feature a manual adjustment 4. knob instead of an automatic adjustment system. They are great for those who need precise control over the size and depth of their wire strips.

Adjustable Wire Strippers

These are designed with adjustable blades that can be set to any size wire you need to strip. They feature a comfortable handle and adjustable jaws that make it easy to strip different sized wires quickly and accurately.

Manual Wire Strippers

These essential tools require manual effort to strip insulation from electrical wires. They feature simple designs with adjustable blades that allow you to customize the size and depth of your wire strips. These types of strippers are great for those who don't need a lot of precision when stripping wires.

Parts of a Wire Stripper

 

  1. Handle: This is the part of the wire stripper you hold onto.
  2. Blades: These are the sharp edges of the wire stripper that cut through the insulation on the wire.
  3. Adjustable Stop: This piece of metal is small and adjustable, which enables you to set the depth of cut for each wire size.
  4. Jaws: The jaws hold the wire while you strip it. They come in various sizes to fit different gauge wires.
  5. Wire Guide: The wire guide is a small hole that helps guide and center your wire as you strip it.

Factors to Consider When Choosing a Wire Stripper

When choosing a wire stripper, there are several factors to consider. First, think about the type of wires you’ll be stripping and the size range you need. You should also consider how often you’ll be using the wire stripper and whether you need a model with adjustable blades. Finally, think about your budget and how much you’re willing to spend on a wire stripper.

Frequently Asked Questions About Wire Strippers

How to use a wire stripper?

To use a wire stripper, first select the correct tool size for the size of the wire you are working with. Place the wire in the tool and squeeze the handles together to cut off the insulation from the wire. Then, adjust the tool to fit around the exposed wire and squeeze again to remove more insulation. Repeat this process until all the insulation is removed from your desired length of wire.

What types of wire cutters are there?

There are several types of wire cutters available on the market, including diagonal pliers, side-cutting pliers, flush-cutting pliers, and cable cutters. Each type has its unique design and purpose for cutting different wires.

What is a wire stripper?

A wire stripper is a hand-held tool used to strip away insulation from electrical wires. It can be used to remove insulation from multiple wires at once without damaging them.

What are wire strippers used for?

Wire strippers are primarily used for electrical wiring projects, such as installing new outlets or switches. They can also be used for other projects, such as stripping away insulation from wires before soldering them together or stripping away rubber casing from cables.

What do wire strippers look like?

Wire strippers typically have two handles that open and close like scissors when squeezed together. The end of one handle will have an adjustable jaw that can be adjusted to fit different sizes of wires. The other handle will have a blade that is used to strip away insulation from the wires.

Wire strippers are a useful tool for any electrical project. There are several different types of wire strippers available, so it’s important to choose the right one for your particular needs. Consider the type of wires you’ll be stripping, the size range you need, how often you’ll be using the wire stripper, and your budget before making a purchase.

Product Compliance and Suitability

The product statements contained in this guide are intended for general informational purposes only. Such product statements do not constitute a product recommendation or representation as to the appropriateness, accuracy, completeness, correctness, or currentness of the information provided. Information provided in this guide does not replace the use by you of any manufacturer instructions, technical product manual, or other professional resource or adviser available to you. Always read, understand, and follow all manufacturer instructions. Portions of this article were generated in part by ChatGPT, and edited by a member of the Zoro team.

Related Articles