Latching Relays (25 items)
Enclosed Mech Latching Relay, 20A
Latching Relay
Enclosed Mech Latching Relay, 20A, SPST
Mechanically Latching Relay, 12Vac/DC
Mechanically Latching Lighting Rly, 24 Vac/dc Coil, SPST relay w/5540W
Enclosed Mech Latching Relay, 20A, SPST
Relay, 24 Vac/dc Coil, 5540W; 277Vac In, 20A; 120-277Vac Bal and 16A
LTG DIN Rail Latching Relay 20Amp Polarized 24V w/ Status
LSBW-2C-24A = 1/2 LATCH 2 POLE
Mechanically Latching Lighting Relay, 24 Vac/dc Coil, SPST relay with
LTG DIN Rail Latching Relay 20Amp Polarized 24V
Enclosed Relay, 20A, SPST
Enclosed Mech Latch Relay, 20A
Latching Relay, w/Switch, 24Vac/DC
LS-9523M = DPDT LATCHING RELAY
About Latching Relays
Latching Relays are electrical devices that allow for the control of an electrical circuit. They can be used to switch between two different states and are commonly used to control the flow of power. There are a variety of Latching Relays available, such as 12 volt latching relay circuits, 2 coil latching relay circuits, 24vac latching relays, ac latching relays, and mechanical latch relays.
Types of Latching Relays
Latching Relays come in various shapes and sizes depending on their purpose. For example, electrically latched relays have a low current draw when in their "off" state while pulse latching relays rely on pulses to switch between states. Additionally, SPST (Single Pole Single Throw) Latch Relay is commonly used to maintain a single state while Schneider Latch Relay is often used when multiple contacts need to be controlled.
How Latching Relays are Made
The majority of Latch Relay designs use electromagnetism or mechanical components such as levers or springs for operation. Electromagnetic designs usually consist of coils wound around iron cores with an armature that can be attracted by the magnetic field created by the coil when energized. Mechanical designs may use an armature or lever connected to a spring which stores energy until it is released through manual or automated means.
Industries that use Latching Relays
Latch Relay switches are often found in industrial settings where they may be used for controlling machinery or process control applications. Professionals who work in manufacturing plants and production lines will often make use of these devices as they provide reliable switching capabilities with minimal power consumption. In addition, latch relaying technology is also widely utilized within medical equipment and home automation systems.
Find the Latching Relays You Need at Zoro
Looking for a specific item? Use our robust search tool to find it by name or keyword, or use our handy filters to narrow down our full assortment. You can also check out our whole selection of electrical supplies, along with other tools or equipment to ensure you have all you need to tackle the job, especially if you're taking on a DIY project for the first time. Plus, when you shop at Zoro, you'll always enjoy competitive prices on tons of great brands you know and trust. We make the shopping experience as fast and seamless as possible with free shipping on orders over $50 for registered users, Net 30 payment terms for qualifying customers, and an unparalleled customer service experience.